Skip to main content
Piranha
Principal III
Sep 28, 2019 11:10 PM UTC
Question

How to make Ethernet and lwIP working on STM32

This is an umbrella topic where I will collect the key problems and solutions to finally get networking on STM32 working. The issues formatted as bold are the most critical ones.

HAL ETH drivers have been significantly reworked since the following firmware packages: CubeF4 v1.27.0, CubeF7 v1.17.0, CubeH5 v1.0.0, CubeH7 v1.10.0

Series: F1, F2, F4, F7, H5, H7 (all STM32 with Ethernet)

Series: F1, F2, F4, F7 (older Synopsys basic peripheral)

Series: H5, H7 (newer Synopsys QoS peripheral)

Series: F7, H7 (Cortex-M7 CPU)

lwIP API related:

Other related information:

Another detailed topic by @alister​: "[bug fixes] STM32H7 Ethernet". While mostly dedicated to H7 series, it also has a good amount of information relevant to all Ethernet/lwIP related development.

Open source zero-copy Ethernet/lwIP driver example. The hardware driver is for F2 series, which means that it's almost the same for all Fx series. The lwIP related code and general ideas are still valid for all series.

My other closely related topic: "Actually working STM32 Ethernet and lwIP demonstration firmware". As that topic is currently unavailable, because ST still has not moved it to the new forum, I am attaching a PDF copy of that topic and the related firmware files to this topic.

This topic has been closed for replies.

27 replies

Piranha
PiranhaAuthor
Principal III
Oct 2, 2019 1:03 PM UTC

As the main topic has hit a 10000 character limit, I'm changing this message to a list of fixed issues, which many people will still find useful.

Series: F1, F2, F4, F7 (older Synopsys basic peripheral)

Series: H7 (newer Synopsys QoS peripheral)

Series: F7, H7 (Cortex-M7 based)

  • lwIP driver Rx data buffers not aligned to cache line size. The address and size of buffers, on which D-cache invalidation is done, must be aligned to __SCB_DCACHE_LINE_SIZE, which is 32 bytes for Cortex-M7. Instead of doing D-cache maintenance, newer ST provided code uses MPU to configure specific memory regions as non-cacheable. It's a very poor solution performance wise, but at least it is functionally correct. For a proper and decent solution it is recommended to read my article "Maintaining CPU data cache coherence for DMA buffers". [Fixed by using MPU.]
SKana.3
Visitor II
Aug 24, 2021 9:30 AM UTC

Hello, Piranha.

I read many of your messages about Ethernet driver for LWIP.

I use NUCLEO-767ZI and I use BSD sockets and therefore FreeRTOS.

For NUCLEO-767ZI I wrote code and it work fine. But I decide move project on NUCLEO-H755. And I start fight with MPU and others...

Amel NASRI
ST Technical Moderator
Oct 4, 2019 2:54 PM UTC

Hi @Piranha​ ,

Needed follow-up actions for each discussion are tracked internally by me & Imen.

I suggest to close the current question.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Piranha
PiranhaAuthor
Principal III
Dec 3, 2019 9:31 AM UTC

I've added substantial amount of new information.

ranran
Senior
Dec 3, 2019 7:28 PM UTC

Hi Piranha,

Thank you very much for the information.

If I may please ask why you don't share the sources ? I will try to do the modifications for H7.

Thanks

nguen nguyen
Associate III
Jan 6, 2020 2:00 PM UTC

Can anyone send example project ? thanks so much Cubemx 5.4

alister
Senior III
Feb 12, 2020 9:59 PM UTC

My fixes and improvements to ST's STM32H7 ETH driver and lwIP ethernetif.c are at https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet.

Source code and documentation attached.

I don't use evaluation boards or build example code.

You'll have to port my changes yourself.

anotherandrew
Senior
Jun 2, 2020 2:27 PM UTC

Thank you @Piranha​ for this detailed write-up! I've updated the original thread to point to this one. *excellent* information and lots of detail.

JBerry
Associate II
Aug 26, 2020 8:03 PM UTC

I am attempting to get Ethernet work on an STM32H745 on the M7 core currently. But I am using CubeIDE 1.4.2 and CubeMX 6.0.1 with ver 1.8.0 of the H7 firmware package. Since these are a bit newer, it is unclear to me which of these issues are still present and which still need fixing. Does anyone have any updates that apply to the newer stuff?

MTros.1
Associate II
Sep 2, 2020 6:17 AM UTC

Yes, I think same as you. It is worthy to make it clear which ones have remained until now.

alister
Senior III
Sep 3, 2020 2:11 AM UTC

@JBerry​ , @MTros.1​  this is a community forum and as you're presently working on H7 ethernet and using H7_FW v1.8.0, and as Piranha may also have a day job and mightn't be working on either, perhaps you're best positioned to do this investigation and contribute the answers.

I'd documented and fixed/improved the H7_FW v1.5.0/v1.6.0 ethernet problems at https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet. It's valid for v1.7.0 too.

I haven't the time to read H7_FW v1.8.0 now. Could you read the the issues I'd documented and fixed/improved there, compare the fixes, and read the issues Piranha's posted here, and post the results of your analysis there and here please?

DMann.1
Visitor II
Sep 26, 2020 10:19 PM UTC

Are you saying the current release of LWIP and FreeRTOS do not work at all without bug fixes, or just simply inefficient and bugs are present?

Mikk Leini
Senior
Dec 20, 2020 5:23 PM UTC

I stumbled upon this STM32 LwIP disaster also and after 1w of swearing and debugging, moved over to Mbed with my F7 device. Mbed TCP/IP stack and OS works out of a box. I'm still in mid development but haven't seen any network issues. But the grass is not bright green there either - the list of debuggable MCU's is quite short. Need dual project solution with shared code to get the job done. Develop and debug HW level code in STM32CubeIDE and run whole application in Mbed.