STM32 MCU errata sheets: Expected preliminary updates
- Oct 12, 2026 10:01 AM UTC
- 0 replies
- 5077 views
Introduction
This article includes preliminary updates of STM32 MCU errata sheets reported since 1st January 2024. It highlights the current description requiring update and the expected one if available.
The purpose of this article is to deliver any expected updates to our MCU errata sheets prior to actual documentation releases. We wish to be transparent with our updates and provide them as fast as possible, to assist you in your design process.
This article is updated on a quarterly basis. Once these preliminary updates are manifested in the errata sheets, this article is refreshed with new information.
Moving forward, we are also working on providing errata sheet releases on a more frequent basis.
IMPORTANT NOTICE - READ CAREFULLY:
- STMicroelectronics NV and its subsidiaries (“ST”) reserve the right to make changes, corrections, enhancements, modifications, and improvements to this article at any time without notice.
- Information in this article supersedes and replaces information previously supplied in any prior versions of this article.
- The following table gives a quick reference to the preliminary documentation updates which may be changed or improved without notice.
- This article will be reviewed on a quarterly basis and applied updates will be removed from the table.
- The hyperlinks under "Doc Reference - Revision" provides a direct link to the specific document page where the description is located.
Summary of documentation updates: "STM32 MCU errata sheets"
| Function | Series/Lines | Doc Reference - Revision | Description | Date of added update |
| System | STM32G471xx | (Jun 2024) | Remove section: The same errata looks to appear 2 times : 2.2.5 MCU cannot enter in Standby mode when HSE bypass used | Jun 2025 |
| STM32H723xx STM32H730xx STM32H733xx STM32H725xx STM32H735xx | ES0491 Rev9 (Jun 2024) | Add section: Description: When HASH transfers data using a channel from DMA1 or DMA2, utilizing another channel from these DMAs to manage other peripherals can cause HASH input data corruption. Workaround Apply one of the following measures: • During a HASH data transfer using DMA1, make sure that no DMA channels are enabled on DMA2 (and vice versa). Additionally, set bit 20 in the DMA_SxCR register, where 'x' is the channel used for HASH data transfer. • Use the interrupt or polling mode to transfer data to the HASH peripheral when DMA1 or DMA2 channels cannot be disabled during the HASH transfer. | Sep 2026 | |
| STM32N6 | Aug 2026 | Add section: TCM ECC Initialization Required Before First Use Description Chapter SRAM and its ECC subsection describe the ECC behavior for SRAM memories. However, it is not explicitly stated that the TCM memories (ITCM/DTCM) also implement ECC protection and require an initialization phase before their first use. The ECC management of the TCM is performed by the Arm Cortex-M55 CPU. When a TCM location has not been initialized, its ECC bits contain undefined values. A read access performed before the first write to the corresponding location may therefore generate an ECC error. As described in the Arm Cortex-M55 Processor Technical Reference Manual (r0p2), ECC memory protection behavior and error detection/processing, all ECC-protected TCM locations must be initialized before being accessed by load instructions. Impact If DTCM memory is accessed before initialization:
Workaround Example workaround startup code /***************** Code to be added - start ***********************/ /* Call the clock system initialization function. */ | Sep 2026 | |
| IWDG | STM32F100x4 STM32F100x6 | (Jul 2022) | Remove sections: Delete duplicated sections: - RVU flag not cleared at low APB clock frequency - PVU flag not cleared at low APB clock frequency | Mar |
| STM32F10xx4 STM32F10xx6 | (Jun 2022) | |||
| STM32F101xF | (Jul 2022) | |||
| STM32F101xC | (Jun 2022) | |||
| STM32F105xx STM32F107xx | (Jun 2022) | |||
| STM32F100xC STM32F100xD STM32F100xE | (Aug 2022) | |||
| HRTIM | STM32F334x4 | (Aug 2021) | Table 4. Summary of silicon limitations Current:
A = limitation present, workaround available Expected: With N = limitation present, no workaround available | Nov 2024 |
| ADC | STM32L412xx | ES0456 Rev6 (Nov 2024) | Remove section: Delete duplicated section: "2.6.9 Writing ADCx_JSQR when JADCSTART and JQDIS are set might lead to incorrect behavior" should be removed. It is duplicated with "2.6.1 Writing ADC_JSQR when JADCSTART and JQDIS are set may lead to incorrect behavior" | Dec 2024 |
| STM32G491xx STM32G4A1xx | (Jun 2024) | Update section: 2.5.11 An ADC instance may impact the accuracy of another ADC instance at specific conditions Expected: ![]()
| Jun 2026 | |
| STM32G431xx STM32G441xx | (Jun 2024) | |||
| STM32G471xx STM32G473xx STM32G474xx STM32G483xx STM32G484xx | (Jun 2024) | Update section: 2.7.11 An ADC instance may impact the accuracy of another ADC instance at specific conditions Expected: ![]()
| Jun 2026 | |
| CEC | STM32H7A3xI STM32H7A3xG | ES0478 Rev11 (Apr 2022) | Add section: Unexpected TXERR flag during a message transmission. Description During the transmission of a 0 or a 1, the HDMI-CEC drives the open-drain output to high-Z, so that the external pull-up implements a voltage rising ramp on the CEC line. | Dec 2024 |
| OCTOSPI | STM32H7A3xI STM32H7A3xG | ES0478 Rev11 (Apr 2022) | Add section: Transactions are limited to 8 Mbytes in OctaRAM™ memories. Description When the controller is configured in Macronix OctaRAM™ mode, by setting the MTYP[2:0] bitfield of the OCTOSPI_DCR1 register to 011, only 13 bits of row address are decoded and sent to the memory, meaning that only 8 K of 1-Kbyte blocks can be accessed (8 Mbytes). | Dec 2024 |
| Applicability | STM32H7A3xI STM32H7A3xG STM32H7B0xB STM32H7B3xI | (Apr 2022) | Table 1. Device summary Add: STM32H7A3LG in the part numbers list. | Jun 2025 |
| TIM | STM32F105xx STM32F107xx | (Jun 2022) | Remove section: Delete duplicated sections - PWM re-enabled in automatic output enable mode despite of system break - TRGO and TRGO2 trigger output failure - Consecutive compare event missed in specific conditions - Output compare clear not working with external counter reset | Jun 2026 |
| STM32F10xx4 STM32F10xx6 | (Jun 2022) | |||
| Summary of device errata | STM32F058C8 STM32F058R8 | (Oct 2020) | Add in Table 2. Summary of device limitations: 2.2.1 Wakeup sequence from Standby mode when using more than one wakeup source | Jun 2026 |
| STM32H723xx STM32H730xx STM32H733xx STM32H725xx STM32H735xx | ES0491 Rev9 (Jun 2024) | Add note in table 3 for 2.2.3 Secure firmware install (SFI): 1. This erratum is fixed in part numbers with RSS version 3.1.0 associated to bootloader revision 9.3. It is present in part | Sep 2026 | |
| USART | STM32WLE5xx STM32WLE4xx | (Mar 2023) | Add in Table 2. Summary of device limitations: 2.8.2 Data corruption due to noisy receive line | Jun 2026 |
| RTC and TAMP | STM32H723xx STM32H730xx STM32H733xx STM32H725xx STM32H735xx | ES0491 Rev9 (Jun 2024) | Add section: Some reference manual revisions may wrongly mentioned the PCx MODE and value while it is reserved. | Sep 2026 |