Skip to main content
AAshc
Associate
Nov 20, 2019 1:26 PM UTC
Solved

Hello! May be it is wrong ethernet DMA tail calculation?

In ethernet HAL driver stm32h7xx_hal_eth.c function void ETH_DMARxDescListInit include row: " WRITE_REG(heth->Instance->DMACRDTPR, ((uint32_t)(heth->Init.RxDesc + (((uint32_t)(ETH_RX_DESC_CNT - 1))*sizeof(ETH_DMADescTypeDef)))));"

This code adding value to heth->Init.RxDesc. But, RxDesc is pointer to 32bit and added shift is multiplicated for 4.

Correct row must be:

" WRITE_REG(heth->Instance->DMACRDTPR, ((uint32_t)(heth->Init.RxDesc) + ((uint32_t)(ETH_RX_DESC_CNT - 1))*sizeof(ETH_DMADescTypeDef)));"

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
Nov 20, 2019 6:08 PM UTC

Created an issue on github:

https://github.com/STMicroelectronics/STM32CubeH7/issues/7

Yep, this is why "better" languages like Go don't have pointer arithmetic. Too confusing. Causes more trouble than utility.

-- pa

14 replies

Pavel A.
Nov 20, 2019 3:59 PM UTC

RxDesc is pointer to ETH_DMADescTypeDef. 6*4 bytes,

-- pa

Piranha
Principal III
Nov 20, 2019 5:44 PM UTC

Pavel is right - RxDesc is a pointer to a structure. Therefore neither ST's, nor your version is correct because of C pointer arithmetic, but the correct version is even simpler:

WRITE_REG(heth->Instance->DMACRDTPR, ((uint32_t)(heth->Init.RxDesc + (uint32_t)(ETH_RX_DESC_CNT - 1))));

ST, this is a bug report and we're talking about this line:

https://github.com/STMicroelectronics/STM32CubeH7/blob/e261d820b398846a94f22f4aeb32d86c29546efb/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_eth.c#L2704

P.S. ST's driver developers, who don't know C pointer arithmetic? Fabulous! Do they know arithmetic at all?

waclawek.jan
Super User
Nov 20, 2019 5:49 PM UTC

@Piranha ,

@AAshc​ 's version is correct, too, as he casts the pointer to integer before applying the + operator, and then uses sizeof() of the target type.

I personally am not fan of pointer arithmetics, as it's bit easily perceivable when fast reading code; and I recommend to explicitly comment all instances where it's used, or, maybe better, use it in the &a[b] form, which is more easily recognizable when reading the code.

(Strictly speaking, pointer cast to integer is not entirely correct, but then all three versions do some form of that).

JW

Piranha
Principal III
Nov 20, 2019 6:03 PM UTC

Indeed, I stand corrected! I overlooked the braces in OP's version. Therefore only ST's version is flawed.

waclawek.jan
Super User
Nov 20, 2019 11:53 PM UTC

I don't really care as I don't Cube, but is this limited to H7?

JW

Piranha
Principal III
Nov 21, 2019 6:44 PM UTC

Yes, H7 only. Other STM32 series doesn't even have that or similar register. H7 has a different ETH peripheral than all other STM32 MCUs.

waclawek.jan
Super User
Nov 21, 2019 9:03 PM UTC

Oh, I see. Thanks for the explanation.

JW

Piranha
Principal III
Feb 2, 2020 9:58 AM UTC

By the way, here is the respective code line from H7 HAL v1.3.0:

WRITE_REG(heth->Instance->DMACRDTPR, ((uint32_t)heth->Init.RxDesc + ((ETH_RX_DESC_CNT - 1)*sizeof(ETH_DMADescTypeDef))));

It's essentially the same as the OP's version. It relied on C operator precedence, but it was correct! Until some brainless code monkey "fixed" it by adding braces in wrong places...

LCE
Principal III
Jan 10, 2023 7:08 AM UTC

I'm just changing my non-HAL ethernet driver from F7 to H7 - oh my, it is so different.

At start, why not set the tail pointer directly to the last descriptor's address?

ETH->DMACRDTPR = (uint32_t)&DMARxDscrTab[ETH_RX_DESC_CNT - 1];

But maybe I have not yet fully understood the tail pointer.

Thankfully I found this thread with @alister​ 's explanation.

https://community.st.com/s/question/0D53W00000EGsnUSAT/how-does-ethernet-rx-descriptor-wrapping-work-on-stm32h7