Skip to main content
GHoll.2
Visitor II
September 6, 2022
Question

PTP clock source is SYSCLK or HCLK?

  • September 6, 2022
  • 3 replies
  • 1880 views

The reference manual for STM32F407 shows (RM0090) that the PTP clock is running from the SYSCLK directly, however, the PTP chapter says that it is controlled by the HCLK. I'm confused now, and experiments show that it is running from HCLK actually. So either the clock diagram in the chapter 7 is wrong (and also CubeMX) or I misunderstand something. Can I drive PTP clock from SYSCLK?

This topic has been closed for replies.

3 replies

KDJEM.1
ST Technical Moderator
December 19, 2022

Hello @Gergely Hollósi​ welcome to the Community :),

Thank you for bringing these issues to our attention.

The PTP clock source is the HCLK.

I reported Internally.

Documentation related issue tracked under the number 141623. 

STM32CubeMX issue tracked in internal ticket 141633.

These are internal tracking numbers and are not accessible or usable by customers.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Piranha
Principal III
December 20, 2022

As always, I remind that obviously the same issue must be checked and updated for all F1, F2, F4, F7 series MCUs with ETH peripheral in reference manuals and CubeMX.

KDJEM.1
ST Technical Moderator
December 20, 2022

Hello @Piranha​,

Thanks for bringing this issue to our attention.

I reported internally.

Thank you

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.