2024-09-04 09:16 PM
Hi Team,
ST-Link Connection Issues with STM32F072RBT6 Discovery Board
Hi everyone,
I’m experiencing issues with my STM32F072RBT6 Discovery Board. It was working fine until recently when I started encountering errors with the ST-Link debugger.
Error Details:
I have attached screenshots of the errors for reference.
Steps I Have Tried:
PFA (images)below including stm32cubeprogrammer logs.
Despite these efforts, the issue persists. Any advice or suggestions on how to resolve this problem would be greatly appreciated. Thank you!
Best regards,
Sudharshan
2024-09-05 03:05 AM
So it's losing connection to the device.
Does your application put the CPU to sleep, and/or disable or reconfigure the SWD pins?
2024-09-05 03:34 AM
Hi,
The application/code doesn't put the CPU to sleep . The flashing or debugging is using a ST-Link (a USB wire). In STM32CubeIDE , during debug mode , i am facing this issue . Could you explain the disable or reconfigure the SWD pins mean here ?
Thanks
Sudarshan
2024-09-05 03:45 AM
@Sudharshan wrote:Could you explain the disable or reconfigure the SWD pins mean here ?
The SWD lines (SWDIO and SWCLK) are on PA13 and PA14:
So, if your code does anything to PA13 and/or PA14, it will break the debug connection.
https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/ta-p/49693
2024-09-05 06:08 AM
Maybe hold BOOT0 high during reset, then connect over SWD with STM32CubeProgrammer.