Associate III
September 5, 2024
Question
unable to connect STM32F072RBT6 via stlink (usb cable )
- 6 replies
- 2103 views
Hi Team,
ST-Link Connection Issues with STM32F072RBT6 Discovery Board
Hi everyone,
I’m experiencing issues with my STM32F072RBT6 Discovery Board. It was working fine until recently when I started encountering errors with the ST-Link debugger.
Error Details:
- During Debug Mode: The debugger displays the error message "TARGET HALT" and disconnects.
- Flashing Code: When trying to flash the code, I receive the error "Debugger Disconnected."
- STM32CubeProgrammer: I also get a warning message saying "Connection to device 0x448 is lost," followed by "Disconnected from device."
I have attached screenshots of the errors for reference.
Steps I Have Tried:
- Verified hardware connections.
- Reset the STM32 board.
- Updated ST-Link firmware.
- Checked STM32CubeProgrammer and STM32CubeIDE settings.
- Confirmed stable power supply.
- Looked for hardware issues on the board.
- Attempted a full chip erase via STM32CubeProgrammer.
PFA (images)below including stm32cubeprogrammer logs.
Despite these efforts, the issue persists. Any advice or suggestions on how to resolve this problem would be greatly appreciated. Thank you!
Best regards,
Sudharshan