ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to use "NFC Tap" -> "CoreNFC" -> "Custom"

I thought I could send custom commands to the ST25DV Tag by using the NFC Tap app. Is that possible?In the app there are two fields when I chose "Custom":1) Custom Command. There I enter "AC", to Read Message (mailbox).2) Data: what to enter here? Ca...

JDirk.1 by Senior
  • 2644 Views
  • 7 replies
  • 0 kudos

ST25DV04 WITH STM32WB READ GARBAGE VALUE

I'm USING ST25DV04 WITH STM32WB THROUGH 12C BUS.IAM ABLE TO WRITE FROM MCU AND READ IT IN APP,AND ALSO ABLE TO WRITE THROUGH APP INTO THE MEMORY,BUT COULDN'T READ THE SAME THING WHAT I WRITE IN THE APP.I CAN ONLY READ SAME GARBAGE VALUE OR ZERO

NASOK.1 by Associate II
  • 554 Views
  • 1 replies
  • 0 kudos

Resolved! Here is my code to add the SPI function. But undefined reference to 'HAL_SPl_Init'.

�?��?空隙MX_SPI2_Init(空隙)#include "app_nfc7.h"/* Private includes ----------------------------------------------------------*//* USER CODE BEGIN Includes *//* USER CODE END Includes *//* Private typedef -------------------------------------------------...

Resolved! Why ST25PC-NFC program crashing on windows 10?

I am using ST25DV64KC and ST25PC-NFC v 2.61 on my pc with windows 10. The software opens just for few seconds and then closes by itself. I have installed it thrice. I tried restarting my pc as well but nothing helped. Kindly let me know what can i d...

NZama.1 by Associate III
  • 1308 Views
  • 5 replies
  • 0 kudos