Hi to all.I should make an application with NFC where the entire circuit is powered by energy harvesting.For this reason I thought of using the ST25DV and I have already purchased the ST25DV_Discovery_C1 and ST25DV_Discovery_C6On these discovery I cl...
Posted on October 27, 2017 at 15:58hello i have download the library for NFC 'en.x-cube-nfc5' and i running the demo example. i can read read the unique id from nfc card, but i cannot find a way to read ndef message. how can i do it?thanks #st25r...
Hello,I made my own board with a ST25DV64K and a microcontroleur STM32L031K6. I would like to put in the NFC tag a NDEF message (URL/text...). For the moment, I don't use the microcontroleur. I use the Android App ST25, built by ST, to put the NDEF m...
Error - 8700 : Frame wait time out OR no tagEven though a writeis succesfull, I will at one time get this error code back (this is the answer of the SendReceive, the result of SendReceive itself is errorcode '4 ' which stands for Communication Error)...
Hi!I use M24LR64E supplied with 3V3 and communicating with PIC microcontroller.I am facing a big and urgent problem: I2C writes are working really fine according to manual specification until the memory is subjected to EMI. After that, any I2C write ...
Error message is c:/eclipse/plugins/fr.ac6.mcu.externaltools.arm-none.win32_1.17.0.201812190825/tools/compiler/bin/../lib/gcc/arm-none-eabi/7.3.1/../../../../arm-none-eabi/bin/ld.exe: region `RAM' overflowed by 957840 bytes.Output.map tells_estack = ...
Hello community, am writing here because I need support in designing an RFID-based system.At current stage I have settled on the ST25RU3993 IC as an RFID reader. However, I can't understand if and how an antenna should be connected to the IC.Can anyb...
After migrating to Nordic-nrf52832 platform with STM32CubeExpansion_NFC5_V2.0.0, I can initialize successfully (all initialization processes can succeed), and fail to Polling Tag Detect.Refer to the example completely for program running processint m...