ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST25R3911B and Arduino SPI not working

Hi,I am trying to get an SPI connection working with my Arduino UNO and the ST25R3911B. I am trying to read the identity register 3Fh but am not getting a response on MISO.My setup is as follows:*VDD & VDD_IO connected with 5V from the Arduino UNO wi...

0693W000008xqMiQAI.png
MMcAl.1 by Associate III
  • 1699 Views
  • 8 replies
  • 0 kudos

Resolved! Reading UID of iclass HID card using st25r3911b

we are trying to use st25r3911b to read UID of iclass HID dy card we have, we can see st25r3911b wake up once card is in range, but the rfalNfcPollTechDetetection is not able to detect any technology (we activated detection of all technologies). How ...

mohamed2 by Associate II
  • 1222 Views
  • 1 replies
  • 0 kudos

Resolved! PC Software supporting other NFC Writer?

Dear All, is there a possibility to implement another driver for other commercial reader/writer like the uTrust 3720 into the Software STSW-ST25PC001, or a way to implement it by myself with the STSW-ST25PC002?Or where can I purchase the Feig control...

APayo.1 by Associate II
  • 672 Views
  • 1 replies
  • 0 kudos

Resolved! What product should I choose to use a custom antenna

Hello everyone, I am working on a project in which I will use NFC tag. I though to use ST25R shield for nucleo board but I need a product on which I can use my own antenna and my own matching circuit. Do you have advice on which product to choose ? T...

Mc3 by Associate II
  • 1204 Views
  • 4 replies
  • 0 kudos

Resolved! ST25 NFC READ/WRITE command

HelloWe are currently developing nfc with 'ST25R3916-DISCO'.​Software is using STSW-ST25R011.​​I got curious as I analyzed the code.​Can I change the command of read/write?​ex) write  command : A2 04 ...Hello​We are currently developing nfc with 'ST...

LJooS.1 by Associate II
  • 812 Views
  • 1 replies
  • 0 kudos

Resolved! CR95HF: Intermittent Invalid Protocol - 0x83

Hello Folks, We intermittently see an "invalid protocol - 0x83' error while reading data.send_cmd 0x04 0x04 0x16 0x00 0x00 0x00rcv_hdr 0x83 0x00This happens intermittently and I have not been successful in reproducing the error. Usually a restart or ...

ABirj.1 by Associate
  • 625 Views
  • 1 replies
  • 0 kudos