Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C Debugging with Platformio

Hi everyone: i received in these days a custom PCB i designed based on the STM32F411 microcontroller:I wanted to experiment with such MCUs and make a custom board with them for the first time; i was also interested in making it compatible with the ar...

Resolved! Why are my PCB traces overheating during testing?

Hey folks, I’m new to PCB design and I ran into something odd. I had a small board made for a project, but during testing some of the traces get warm and one even browned slightly. I thought I sized them correctly in KiCad, but maybe I messed up.Do P...

Kasuo by Associate II
  • 681 Views
  • 3 replies
  • 1 kudos

Resolved! PLC module with ADC and mcu

Could you please suggest a PLC module that includes a signal scaling unit and an isolation circuit, equipped with a high-speed sampling ADC with up to 16-bit resolution? The module should also integrate a microcontroller featuring SPI, LAN (Ethernet)...