Skip to main content
Associate
December 4, 2024
Question

smd marking

HELLO. CAN SOMEONE HELP ME IDENTIFY THIS CIRCUIT WHICH HAS THE NOTATION OF L4T . IT APPEARS TO BE A MOSFET BUT I'M NOT SURE BECAUSE I CAN'T FIND ANY REFERENCE ABOUT IT ANYWHERE. BECAUSE IT HAS 8 PINS. ITS DIMENSIONS ARE 2 X 2 X 1 MM. THANK YOU FOR ANY HELP.

This topic has been closed for replies.

8 replies

December 5, 2024

BAT54W nxp

Associate
December 9, 2024

Hi MMOMO, thank you very much for your answer, the problem is that I can't find any kind of reference about this diode, I don't know how to replace the chip. that is, if I take several diodes, how do I connect them to each other because I have a configuration that feeds me three pins of a microchip, I explain that pin 6 and 7 are connected and arrive at the gnd and have a capacitor up to pin 8, pin 4 is at the gnd , pin 3 is unconnected, pin 1, 2, 7 go to a 74ahc14d. in total, it is about a GILGEN SLA swing gate with microchip type MB96F346RSA. I can't find any kind of diagram for it, hence the problem because I don't know what to replace it with.

Mike_ST
ST Technical Moderator
December 10, 2024

Hello,

You should supply a better photo, instead of taking a picture of a screen. The component is broken enough, there is no need to add difficulty.

Show more of the board so people can feel/guess the purpose of that 8 pins chip.

Maybe follow tracks to see where it is connected, that can help as well.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Tesla DeLorean
Guru
December 10, 2024

Yeah, not sure if is conformally coated or just very messy. Clean with alcohol or solvent.

Try with a smart-phone camera with high MP resolution, and Macro mode.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate
December 15, 2024

(Merged thread)

Thank you once again for your answer. in relation to the chip, unfortunately, when the piece was burned, the first letter was also destroyed, which after my deduction from the remaining half of the inscription I considered to be the letter L. I tried to look for this configuration on the Internet but I couldn't find anything, I think it should be something other than a mosfet and be what you think, a chip with many diodes. I also found this, but there seem to be five versions of it, but not with this inscription on it. I am attaching a diagram, I apologize that it is not very clear.

IMG_L4T3_Cleaned.jpgIMG_L4T2_Clipped.jpg

TDK
December 15, 2024

Can you show the picture of the (burnt) chip?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
December 15, 2024
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..