Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PCB Design & Assembly files for STDES-30KWVRECT

Hello ST Team,   I am working on the STDES-30KWVRECT Vienna PFC rectifier board and I need the following hardware resources:  1. PCB design files (Gerber or Altium project)  2. Assembly drawing with reference designators (for component placement)  3....

Om1 by Associate
  • 659 Views
  • 1 replies
  • 0 kudos

Resolved! Faulty LM358 SPICE model

I'm trying to find a working spice model for the ST LM358. The one on the site gives an output of -12KV for a small sine wave when powered from ± 12VAnd the "contact us" email doesn't work.

CP1 by Associate II
  • 1280 Views
  • 6 replies
  • 0 kudos

Resolved! M24M02E-F only 1 Mbit available?

Hello,We wanted to replace an M24M01-DFCS6 memory (1 Mbit) with an M24M02E-F (advertised as 2 Mbit) available in a WLCSP5 package.After starting the driver implementation, we realized that the sections “Device Type Identifier”, “Configurable Device A...

Image1.png
RomG31 by Associate
  • 866 Views
  • 2 replies
  • 1 kudos

Resolved! STWD100NY Connection

I use STWD100NY Watchdog IC and for now, i can not achieve what i want. The problem is about to get output from the WDO pin. I did not connect the WDO to the MCU but i connect it to drive a relay. I set up my timer to 4 seconds. Even if it exceeds th...

watchdog IC.png