Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Identify this Unknown component.

Hi! I have a cirquitboard that contains a component of ST mark. It is a surficemounted component thatlooks like a diod with a stripe in one end. It is marked DX 63 450 utt i can not find this component onyour side. Can yoy help me?/ Bjoern

Bjoerne by Associate II
  • 791 Views
  • 5 replies
  • 1 kudos

Resolved! 24C256 EEPROM Page Write

Hi there ! I hope someone can help me with a confusion i had in my mind right now. I work with a EEPROM 24C256 and need a write a lot of data inside , soo i decide to use the page write solution . So from the datasheet i saw i can write 64byte in one...

Immagine 2025-09-15 152315.png
SGian.1 by Senior
  • 6899 Views
  • 3 replies
  • 2 kudos

GT9271 TOUCH INT

Hi there. I require assistance to ensure the proper operation of GT9271.After properly RESETting the GT9271, and issuing the 0XBA I2C address, the device keeps pulling the INT pin without any touch on the LCD display (1024x600). I really feel a lack ...

Sem título.png
m-a-c-f by Associate III
  • 5427 Views
  • 13 replies
  • 5 kudos

Resolved! About the operation of the STG3157

”Switch S1 is ON (connected to common port D) when the IN input is held high, andOFF (a high impedance state exists between the two ports) when IN is held low.Switch S2 is ON (connected to common port D) when the IN input is held low andOFF (a high i...

Resolved! Blue and Black Pill SWO debugging

Split from STM32H5 SWO debugging.I want use SWO pin like standalone debug. Send data by "ITM_SendChar('A');" and want to read data from SWO pin by USB-UART dongle, SWO pin => Rx pin UART-USB on PC.I try blue and black pill (STM32F103 and STM32F411), ...

mkigor by Associate II
  • 1735 Views
  • 13 replies
  • 7 kudos