2024-12-10 10:30 PM - last edited on 2024-12-11 12:53 AM by Andrew Neil
Hello everyone,
I am currently using the WM8904 audio codec in my project. The audio is stored in external flash memory, and I am reading it in chunks of 1024 bytes at a time. The audio format is 16-bit WAV with an 8000 Hz sample rate.
For playback, we are using a mono speaker. I have attached the schematic of our codec for reference.
Issue: The audio output is not clear. I have verified the data being read from the flash, and it matches the stored data.
I would like to know:
2024-12-11 12:43 AM
1. read the datasheet of WM8904, which is not a product from ST
2. working source code... you're not telling us which STM32 you are using and how it is connected to the DAC
2024-12-11 1:02 AM
As @LCE said, you need to provide more details - please see the Posting Tips:
@Tharun123 wrote:I have attached the schematic of our codec for reference.
I think you forgot that?
@Tharun123 wrote:Issue: The audio output is not clear.
What, exactly, do you mean by that?
Have you viewed the output on an oscilloscope?
@Tharun123 wrote:
- What audio formats (sample rate, bit width, clock configuration, etc.) are supported by the WM8904 codec?
It's not an ST Product - you need to consult the manufacturer's specifications & other supporting documentation for that:
https://www.cirrus.com/products/wm8904/
https://www.cirrus.com/products/wm8904/#supportRequest=true&formType=design&supportProduct=wm8904
2024-12-19 10:04 PM
sorry for missing details, we are using stm32f407G evaluation board in that there is on board audio codec which is cs43l22 we are storing the audio data in internal buffer which is of 12 kb just for testing purpose.
in stm32 I2S function expects 16 bit data
HAL_StatusTypeDef HAL_I2S_Transmit(I2S_HandleTypeDef *hi2s, uint16_t *pData, uint16_t Size, uint32_t Timeout)
can you have any suggestions how we can store and how we can send the data or is there any library
of audio codec like nxp controllers?
2024-12-20 2:20 AM
@Tharun123 wrote:we are using stm32f407G evaluation board
This: https://www.st.com/en/evaluation-tools/stm3240g-eval.html ?
@Tharun123 wrote:in that there is on board audio codec which is cs43l22
So are there not examples which illustrate the use of it?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.