cancel
Showing results for 
Search instead for 
Did you mean: 

VNLD5160

bestyeng
Associate II

Hi at all.
Can VNLD5160 work with a normal STM32 CPU with 3.3V logical levels?
I don't find this information in datasheet...
Thanks...

1 REPLY 1
Peter BENSCH
ST Employee

Well, the data sheet mentions two important points:

  • Vsupply = VIN = 4.5-5.5V

  • VINTH = 1...3.5V (table 8)

This means that you either use a level translator or configure the GPIO of the STM32 as an open drain with external pull-up. As the VNLD5160 can only switch at a few kHz, the simpler and cheaper open drain variant may be sufficient.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.