The issue about the PD55008-E
Hi,i meeting a issue,I suspect that the parasitic capacitance from the PD55008-E is too large?The waveform output from J500 and the edge is shaking too much.Thanks!
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hi,i meeting a issue,I suspect that the parasitic capacitance from the PD55008-E is too large?The waveform output from J500 and the edge is shaking too much.Thanks!
Edited the post to follow the community guidelines. In next time please use </> button to paste your code. See this post. Hello Experts, I am unable to read the byte of data from eeprom in particular address after written the data.i am getting the r...
I am slowly following along with the user guides and used the software IDE from ST to create a blinker program of the onboard LED. That worked when connected to the ST-Link V2, and it was easy to find the correct pins, but I have the ST-Link V3 set, ...
Is there driver support available for the ST33KTPM on linux / Ubuntu kernel 4.4? ...
I'm using the stm32 board (STM32F103C8T6) the blue pill for testing. I'm just flashing a blinking led code but getting an error Target not found: No stm board found and also getting ST-Link not found after that. Can anyone help me to resolve this iss...
I'm proposing a design using the STGAP2DMTR, and I have the following questions:I) Where can I find a SPICE model of the IC to perform simulations?II) In the datasheet, it is recommended to use 1 µF and 100 nF capacitors for the input and outputs. I ...
Hello, I am currently trying to read the angles from a BNO086 IMU using an STM32 microcontroller (using CubeIDE), and I use this library : https://www.grozeaion.com/electronics/stm32/stm32-i2c-library-for-bno08x-9-axis-imu. The I²C communication seem...
Dear All,can someone, please, specify the meaning of the bit 1 as 'A8' in the I2C address of the M24C04-FMH6TG?I can't find any explanation of this value. Thank you
Hello, is it possible to convert all the codes and libraries of the project into a flowchart that is also editable? Thank you.
Hello, dear ST Please kindly help to provide the body marking surface of M95512-DRMN8TP/K.Thank you!