Skip to main content
Associate II
January 23, 2025
Solved

M24M01E-FMN6TP not able detect the I2c address

  • January 23, 2025
  • 5 replies
  • 1310 views

Hi, 

 

I have made a customized board using STM32 and M24M01E-FMN6TP, but not able to communicate, kindly find the schematic attached. I have written a code for I2c scanner just to test the circuit and it is giving me no i2c device is connected.

I have tested the same in the  customized  breakup board, but still no results. I have also tried connecting E1 and E2 to GND, but still not able to communicate.

 

Kindly guide mw with the solution 

This topic has been closed for replies.
Best answer by Peter BENSCH

You have defined 0x50 for the device address. Do you realise that this is a 7bit address that must be shifted one bit to the left for use? You can find the description in stm32l4xx_hal_i2c.c:

DevAddress Target device address: The device 7 bits address value in datasheet must be shifted to the left before calling the interface

In addition, your pull-ups of 4.7k at SDA and SCL might be too big (you have not yet mentioned the line length or the I2C parameters like the speed). You can also replace them with max. 2.7k, better 1.5k...2.2k. If you don't want to desolder them, you can connect 4.7k each in parallel for a test.

Regards
/Peter

5 replies

Peter BENSCH
ST Technical Moderator
January 23, 2025

Where is the schematics?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Faizan75Author
Associate II
January 24, 2025

Attached

Peter BENSCH
ST Technical Moderator
January 24, 2025

This is just the schematics of the EEPROM and its power supply. Apropos VCC: did you close J10 for testing?

STM32: which one is it and where did you connect the EEPROM?

Please show the source code of how you are trying to access the ERPROM?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Faizan75Author
Associate II
January 24, 2025

Thank you for the reply, Yes i have closed J10 for testing, I have checked voltage across the IC using Multimeter .

 

Currently I am using STM32L476 based microcontroller, Kindly find the sample code attached. I am using i2c1 ( as i have the breakup board to connect to any I2c bus).

 

I have also connected LCD for display.

 

I have also tried using Nucleo-l476RG board connected to my breakup board (EEPROM) and used Arduino IDE to program a simple I2c scanner code, but not able to even detected the EEPROM 

Kindly oblige 

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
January 27, 2025

You have defined 0x50 for the device address. Do you realise that this is a 7bit address that must be shifted one bit to the left for use? You can find the description in stm32l4xx_hal_i2c.c:

DevAddress Target device address: The device 7 bits address value in datasheet must be shifted to the left before calling the interface

In addition, your pull-ups of 4.7k at SDA and SCL might be too big (you have not yet mentioned the line length or the I2C parameters like the speed). You can also replace them with max. 2.7k, better 1.5k...2.2k. If you don't want to desolder them, you can connect 4.7k each in parallel for a test.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.