Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Triac ASC 108 6S FQ41

Bonjour,J’ai un composant qui est détruit sur une carte mère, l’ancienne référence ST est ASC 108 6S FQ41.Pouvez-vous me donner la nouvelle référence qui correspond à ce triac.Je vous remercieBonne journée

Duval by Associate
  • 1984 Views
  • 4 replies
  • 0 kudos

Unknown TSSOP-20 chip identification

Hi all.I'm struggling with certain device and I'd like to identify unknown TSSOP-20 chip on the PCB. Chip must be an MCU and based on the pinout it's very close to some STM8, eg. STM8AF6213. There are VCC and GND connected to Pin 9 and 7 respectively...

MPrih.1 by Associate
  • 3990 Views
  • 4 replies
  • 0 kudos

STHV1600 custom waveform generation

Hi all,I have been testing the STHV1600 evaluation module and want to generate a continuous wave (CW) that would change after some time. Currently, the STSW-IME014 GUI software seems to allow creating multiple CW patterns and assigning them to a spec...

Bartas by Associate
  • 957 Views
  • 0 replies
  • 0 kudos

Configuration of STHV1600

Hello, folks.I'm using the STHV1600 (specifically its evaluation kit board, the STEVAL-IME014V1B) for my thesis on sonothrombolysis. For this ultrasound application, I need multiple time delay configurations for the pulses (approximately 400). The GU...

RHRPMICL1AK01V

Dear, I'm trying to find pricing +  a European distributor that are able to deliverRHRPMICL1AK01V Can anybody help? For the moment, I got no helpful feedback from usual distrubutors Thanks, Nicolas.

IWDG STM8

Hello,STM8S208RB microcontroller, Independent watchdog (IWDG). After starting the watchdog timer (command KEY_ENABLE value = 0xCC), I understand that the watchdog timer stops after resetting the microcontroller. The default register state is undefine...

MykolaLevun_0-1707560153755.png

M95040 Registers definition

Hi,We are using M95040-DFMN6TP SPI PROM on our board.The Serial Input/ Output timing given in the datasheet is not detailed.There is not much info on the address width and data width, and how to control write/read, there also isn't the register defin...

Ravikumar by Associate II
  • 2232 Views
  • 6 replies
  • 0 kudos

Resolved! component identification code 428WP

Hi,  Can anyone help me identify the component(s)?  What kind of components these and what is the type of package (SSOP8 or TSSOP8)? Please see the the pictures. Thank you.    

ST428WP.jpg ST428WP_second.jpg
Gabor1 by Associate
  • 1543 Views
  • 2 replies
  • 1 kudos