User Activity

We are looking to replace our use of M24M02-DR with M24M02E-F as it is available as TSSOP (the smaller CSP would also be useful but it seems no distributor is touching that at the moment) and cheaper (as I guess ST are promoting the replacement of th...
Is there any technical data regarding when the FIFO becomes functional after power up? I have noticed I2C comms and registers can be accessed quite quickly but if the FIFO is initialised too early (e.g. going into FIFO mode), it never starts storing ...
LIS2DE12 (or those similar in range). Reading FIFO I2C. Questions:1) I2C multiple byte read auto-increment. In order to continually read the FIFO with reg address auto incrementing from 0x28 to 0x2D then automatically wrapping around back to 0x28 aga...