cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any option to auto update X-NUCLEO-LPM01A Firmware?

DJohn.16
Associate II

Hi ST family,

I want X-NUCLEO-LPM01A's firmware to auto upgrade. Is there any way to do or we should have to do manually?:grinning_face:

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @DJohn.16​, to the community!

Even though the STM32L496VGT6 included in the kit has a dual bank read-while-write Flash, an auto-upgrade of the firmware would require a special bootloader that supports this and of course a data source including the connection to it from which the upgrade can be obtained. However, the source code for the kit is not available, so you can only upgrade manually.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DJohn.16
Associate II

Nope, Only manual