Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Triac BTA41600B

hey guys,I need to buy a new Triac, the old component is BTA41600B, but there are other letters after this specification, for example: BTA41600B 7SABK VU PHL 7S 135.I would like to know about this feature 7SABK VU PHL 7S 135, as these BTA41600B I fou...

mendonca by Associate
  • 2130 Views
  • 2 replies
  • 1 kudos

IBIS MODEL

Hi Team, We are looking IBIS model for the ITA25B1RL.To simulate SI, required IBIS model. Please provide.Thank you 

Damo by Associate
  • 1101 Views
  • 0 replies
  • 0 kudos

Resolved! Marking STM8L151F3U6TR

Hi, I have bought the parts STM8L151F3U6TR. The marking indicated in datasheet is L526. However, marking on component is L536. Anyone can confirm this marking of L536 is correct? 

Resolved! M24512-W

Hi,I need help to identify a 512 Kbit serial I²C bus EEPROM from the M24512 series.I have two differents parts which appear identical, apart from one letter at the end of the reference : M24512-WG for the first one and M24512-WP for the second (photo...

pepito60 by Associate II
  • 10043 Views
  • 12 replies
  • 8 kudos

eDsim

Hello, i would like to simulate a schematic of a 100W USB PD adapter that include the STUSB4761 usb pd controller using eDsim but i can’t find the controller in the library can any one help me please.

nesrine12 by Associate III
  • 6349 Views
  • 1 replies
  • 0 kudos

L6470

Hi,I am usinga) L6470 to control Stepper motors. I am using STP-MTR-23079(x). The motor has rated current=2.8A/phase, Resisteance=1.1ohm/phase.b) I am using 24VDC for L6470.c) I am setting KVAL = 14.04% with phase current that is around 3.07A/phase. ...

CSu.12 by Associate II
  • 1460 Views
  • 0 replies
  • 0 kudos

Spice Model required for VIPERGAN50TR

Hi,Greetings,I have been using VIPERGAN50TR part quite some time. Now I want run simulation regarding the same.Kindly help me in finding unencrypted spice model.Thanks and Regards,Utham

UV by Associate
  • 1364 Views
  • 1 replies
  • 0 kudos

Cannot access >=3,3V at GPIOA - STM32F411

Dear Ladies and Gentlemen,   for you it is your daily business - for me as customer a contemporary challenge:   Something went wrong with my pin-configuration. I measure ~1,7 V as GPIO-output of Port A instead of wished >=3.3 V. My power supply is a ...

timbo2023 by Associate III
  • 30406 Views
  • 46 replies
  • 20 kudos