Hello,I wonder if somebody can point to or share a driver for Linux 4.x.The current driver at [1] is for Linux 5.4. Since our project is based on a Qualcomm CPU and Qualcomm doesn't provide kernels newer than 4.9, I need a driver for 4.x. Backporting...
Hello: I have a ST EEPROM IC type is "M24C64-F". If I try make write data to the same address over than spec write cycles(4million) , so, does it affect other address's retention data? Does it only affect the data of the address that is written repea...
Our device always use your STM32F413ZG and STMPE811QTR – Resistive touch screen controller, but recently, we found ST only produce one touch screen controller currently, the FTG2-SLP. I do not know you will no longer offer STMPE811QTR or temporarily ...
Hey Folks,I need to put together a statement of volatility for the M95M02-DRMN6TP EEPROM.Does the following accurately reflect the technology and have I missed anything?--Technology: EEPROM Size: 2 Mbit (256 Kbytes) of EEPROM, Page size: 256 bytesCom...
I am trying to use MAC with my STSAFE-A110, in order to further restrict access.I would have expected a function similar to establishing a public key, i.e. StSafeA_PutPublicKeySlot(...), but I can only find StSafeA_PutAttribute.Are we really supposed...
Hi ST Team, i use the SMBJ30A/CA but how much current will be flow if a DC voltage of 40 volt is applied? It must be larger than IBR = 1 mA given in the datasheet. However, there isn't any info for DC operation if a DC voltage above VBR but below VCL...