cancel
Showing results for 
Search instead for 
Did you mean: 

Power dissipation of SMBJ30A/CA for DC operation below clamping voltage

Reha
Associate

Hi ST Team,

i use the SMBJ30A/CA but how much current will be flow if a DC voltage of 40 volt is applied? It must be larger than IBR = 1 mA given in the datasheet. However, there isn't any info for DC operation if a DC voltage above VBR but below VCL is constant applied.  Without this info it is not possible to calculate the power dissipation in the whole path.

Thanks

0 REPLIES 0