Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

doubt eeprom

How long do EEPROM memories used in HDDs retain all data at a temperature of 36°C?EEPROM, like flash, does the number of erases/writes have to do with the data retention time?2.5" and 3.5" HDDs use EEPROM or flash to store BIOS/firmware. What type of...

ÍStef.1 by Associate II
  • 1785 Views
  • 3 replies
  • 5 kudos

Resolved! ST M29W640FT 70N6H doubt

ST M29W640FT 70N6H flash Nor chip with 20 erase write stored in temperature 33-36C and no powered In this case, what is the most approximate and realistic estimate of years for it to retain all the information written on this chip? an approximate num...

ÍStef.1 by Associate II
  • 1270 Views
  • 3 replies
  • 0 kudos

Resolved! EVAL-RHF1201V2

Hello. im currently using the EVAL-RHF1201V2 and would like some help setting it up to properly measure dynamic characteristics. Particularly regarding the RPOL resistance and for a sampling frequency of 40 Mbps and a differential AC input from 1 MHz...

Mo9 by Associate
  • 815 Views
  • 1 replies
  • 0 kudos

Resolved! Questions about M48T201V

Hello,      I am designing with the aforementioned RTC and have the following questions.  I contacted ST support and the solution was to ask the forums.  So here are my questions:What is the date output (i.e. binary, BCD, YY:MM:DD:dd, HH:MM:SS:hh, et...

ST Micro Connection Package

We have an STMC2 in which we have lost the ST Micro Connection Package and cannot use it.Since it is obsolete in STMC2, ST does not have software. Does anyone know where I could download or buy this software?

jmartin by Associate
  • 1092 Views
  • 2 replies
  • 0 kudos