STPS24045 - Product specifications
Hi Team,I would like to know the Part #STPS24045 is qualified AEC. If not, can you help me to get the Diode with a higher current rating (min: 220A of forward current) and AEC qualified. Thanks, in advance.-Gopi
Hi Team,I would like to know the Part #STPS24045 is qualified AEC. If not, can you help me to get the Diode with a higher current rating (min: 220A of forward current) and AEC qualified. Thanks, in advance.-Gopi
Hi again to everyone!I want to know, if somebody know something about this ic´s in the attached pictures (one it´s labeled: "a34 2248", and the other is: "2057 wow1", both in smd structure).It is used to switch beetwin two hdmi signals.I´ve searched...
Hello,I have a question regarding the "STP65N150M9" N-Channel MOSFET. Is there an LTspice model of this component available? If yes, is it possible to gain access to it? Furthermore, I would like to know the following characteristics about this compo...
Hello, I'm new in this community. I have a problem with my control panel from my camper. (Dethleffs) The Control Panel is from Schaudt. It's the MP20-Tproblem: Temperature from both sensors shows -28°feedback from Schaud: The IC is the reason for my ...
Hello everyone,Do any of you still have the ST200 toolset:https://www.st.com/content/st_com/en/support/support-home.htmlbest regardsDanielle
Posted on February 22, 2011 at 09:26Hi Everyone, I made a simple design for AC/DC with VIPer28. How i can't see what is the core (type) of transformer. I print the documentation, but this information is not there. Regards #edesignstudio-simulati...
I’m trying to get streaming data from the following combination:- Device: STHS34PF80- Adaptor: MKI231KA- Motherboard: STEVAL-MKI109V3 I’ve connected a terminal emulator (PuTTY) to the USB port and can connect. I can type the following commands:*setdb...
Hi, I am designing a switching power supply with the STNRG012 integrated circuit and I want to know if the device turns on without the need for an EEPROM memory.
Hellowhere can i find a document witch explain the marking on the EEPROM M24C08-WDW6TThank you
Hello, i am using the SCTWA60N120G2-4 for a traction inverter. It has a HiP247-4 package and of course needs to be cooled. I did not find any information saying that the cooling surface of the package ist isolated or not isolated. Is there any inform...