Skip to main content
Strooom
Senior
April 6, 2024
Solved

Question about Writeprotect (WP) for I2C EEPROM, eg M24M01E

  • April 6, 2024
  • 1 reply
  • 2698 views

For these EEPROMs there is a WP pin, which must be (active) low to enable write operations. I am driving this pin from an MCU, (ie. it is not tied to GND).

Also these EEPROMs need some time after a write command to effectively write the data into the EEPROM, eg. 3.5 ms max.

Now my question is : does the WP need to stay active low during those 3.5 ms after the write command ?

 

This topic has been closed for replies.
Best answer by AScha.3

Ok, you see from timing diagram : /WC has to be lo before write sequence starts and can stay lo or go high after full sequence, including last ACK and I2C STOP .

The eeprom may be busy internal some more time (..4ms) , so you should be sure, not to switch power off in this time.

WC state is no more important here, the internal write is in execution.

And the time, /WC has to be lo after last ACK+STOP , IS in the ds :

AScha3_0-1712410666974.png

 

1 reply

AScha.3
Super User
April 6, 2024

This you should see in the datasheet of your eeprom.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Strooom
StrooomAuthor
Senior
April 6, 2024

Sure, but the datasheet doesn’t answer the question, that’s the reason I ask it here.

Attached is a screenshot of M24M01E-F datasheet. It shows some delay between last I2C databyte and rising WC, but no timing is defined…

I could also try to find out with some experiments, but I prefer a response from someone who knows about the internals of such devices.

AScha.3
AScha.3Best answer
Super User
April 6, 2024

Ok, you see from timing diagram : /WC has to be lo before write sequence starts and can stay lo or go high after full sequence, including last ACK and I2C STOP .

The eeprom may be busy internal some more time (..4ms) , so you should be sure, not to switch power off in this time.

WC state is no more important here, the internal write is in execution.

And the time, /WC has to be lo after last ACK+STOP , IS in the ds :

AScha3_0-1712410666974.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."