Other: hardware

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! M41ST87WMX6TR RTC Vbat Max.

The datasheet states that Vbat max is Vcc. How can this be true if in the case of Vcc absent Vbat will always be greater than Vcc. My assumption is that the author meant that Vbat must not exceed Vcc as specified in the Absolute maximum ratings table...

UB by Associate
  • 385 Views
  • 1 replies
  • 3 kudos

Resolved! M41T93

hi everyone,  Please confirm whether the attached pictures have the same part numbers. Furthermore, could you please explain the meanings of 7C004, 7C006, and 7C008.   BR tehseen Javed

Resolved! diode smd code

Hi everyone,I need help for a smd diode code.E CD C725Is there a datasheet ou other document about? https://drive.google.com/file/d/13dwaZAm-tTzD05-5DyEywvnTxNqFMHIx/view?usp=sharing

Ever76 by Associate
  • 1091 Views
  • 2 replies
  • 1 kudos

Transistor

what is the maximum operating frequency of BDX33 and BDX34 ??

ksoni by Associate
  • 294 Views
  • 2 replies
  • 0 kudos

Image processing processor that supports RGB-IR BAYER

hi all  looking for a MPU that supports the ST VG5671 Camera Unfortunately ST support doesn't have a recommendation for an ST processor that supports an ST camera. Also there  is not a data sheet on their website just a data brief!this produces RGB-I...

PGEEZ1 - Cant write second time

Hi I m using PGEEZ1. Hope you are well. I am going through some irregularities , when i try to read second time it gives me all zeros. Your Assistance will be appreciated!MX_EEPROM_Init();/* USER CODE BEGIN 2 */PGEEZ1_M95P32_WriteEnable(0); printf("\...

Resolved! SMD devices

Hello everyones, what are the red marked devices in smd format, diodes maybe? They are grey and yellow. There are no label on them.

SMusc.1 by Associate III
  • 711 Views
  • 3 replies
  • 1 kudos