Skip to main content
Explorer
March 13, 2024
Solved

M41ST87WMX6TR RTC Vbat Max.

  • March 13, 2024
  • 1 reply
  • 835 views

The datasheet states that Vbat max is Vcc. How can this be true if in the case of Vcc absent Vbat will always be greater than Vcc. My assumption is that the author meant that Vbat must not exceed Vcc as specified in the Absolute maximum ratings table (4.6V), but I would like to have a formal answer for that.

This topic has been closed for replies.
Best answer by TDK

> The datasheet states that Vbat max is Vcc

Clearly a fairly serious typo.

 

Reading through the rest of the datasheet, it is clear that VBAT can exceed VCC. For example, here it is explicitly stated, among other places.

TDK_0-1710345560255.png

 

1 reply

TDK
TDKBest answer
March 13, 2024

> The datasheet states that Vbat max is Vcc

Clearly a fairly serious typo.

 

Reading through the rest of the datasheet, it is clear that VBAT can exceed VCC. For example, here it is explicitly stated, among other places.

TDK_0-1710345560255.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."