Skip to main content
SMusc.1
Associate III
March 6, 2024
Solved

SMD devices

  • March 6, 2024
  • 3 replies
  • 1700 views

Hello everyones, what are the red marked devices in smd format, diodes maybe? They are grey and yellow. There are no label on them.

This topic has been closed for replies.
Best answer by Andrew Neil

Again, don't forget to mark the solution.

BTW: note that "SMD" = Surface-Mount Device - so "SMD device" is a tautology.

See also: LCD display; RAM memory; etc, ...

 

3 replies

TDK
March 6, 2024

 

Those are ceramic capacitors.

"If you feel a post has answered your question, please click ""Accept as Solution""."
SMusc.1
SMusc.1Author
Associate III
March 6, 2024

thank a lot

Andrew Neil
Andrew NeilBest answer
Super User
March 6, 2024

Again, don't forget to mark the solution.

BTW: note that "SMD" = Surface-Mount Device - so "SMD device" is a tautology.

See also: LCD display; RAM memory; etc, ...

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.