cancel
Showing results for 
Search instead for 
Did you mean: 

any inbuild NFC , BLE and Wifi Available in STM32 Controller ?

SKaru.5
Associate II

any inbuild NFC , BLE and Wifi Available in STM32 Controller . or NFC and BLE like that any combination is available ? Please suggest the MCU .

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @SKaru.5​, to the community!

There are currently several STM32 with built-in BLE, also a ready-to-use module including an antenna.

Currently an external module is required for NFC because there are too many combinations that, depending on the function, also have to provide high transmission power.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Guillaume K
ST Employee

for BLE: STM32WB

SKaru.5
Associate II

Thanks for your Reply.

if we select STM32WB for BLE and for NFC Interface any Evaluation Board is available .

NFC - P2P and Reader/Write Mode