Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Default clock speed for Nucleo-8s208RB

HelloWhat clock frequency and timing scheme is used for Nucleo-8S208RB default? In what documentation can I look this up?In the documentation (UM2364 User manual) for the board NUCLEO-8S208RB, this information is written (see picture), but looking at...

picture2.png

Resolved! S2-LP

Hi, I'm working on a pcb for a student designed 3U CubeSat. We are looking at using your s2-lp transceiver. In the datasheet you include an application diagram, however the components are not given any values. Are you able to provide the capacitor an...

adamgarofs_0-1700597371385.png

Resolved! How to access STM8 cpu registers

HelloHow can I access STM8S CPU registers (Cosmic compiler)? When I write this "A = 0xff" (A is a processor register accumulator), then compiler writes this "#error cpstm8 main.c:17(3) A undefined". How to fix it?

Resolved! stm8, cpu register, cosmic

Hello How can I access CPU registers using the Cosmic compiler?For example, when I access register A, the compiler throws an error A is undefined (This is shown in the picture and also the project files).  

picture.png

Vnd7020 self internal diagnostic

Hi community I am working with gate driver vnd7020.I have already implemented the reading of the current (I) for both 2 oyputs and temperature for every chipNow i want to implement the self diagnostic from the driver.I want to detect the overload and...

SGasp1_0-1701163555512.png SGasp1_1-1701163709950.png
SGasp.1 by Senior
  • 805 Views
  • 0 replies
  • 0 kudos