Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Connect to eMoticom eM007 ECU

I have an eMoticom eM007 ECU on a motorcycle which has been developed from the SPC5-L9177A-K02 dev kit. I wish to connect to the ECU to download the bin file so I can learn to tune it. The ECU has a canbus connector with 4 pins +12v, Gnd, CAN-H, and ...

Ian Lowe by Associate II
  • 1460 Views
  • 9 replies
  • 5 kudos

Resolved! Set Life Cycle

I am using the SPC58 MCU product with the TRACE32 debugger. When changing the Life Cycle from "customer_delivery" to "in_field" with the trace32 script, debugging is only possible by entering the keycode. What should I do if I want to change the Life...

hgh by Associate
  • 548 Views
  • 2 replies
  • 1 kudos

Resolved! SPC58EC with Flash driver

Hello, I am currently struggline with flash program with some tools.The tool send 62byte data with CAN FD and I want to write down it.I am using SPC5Studio with Flash_driver (ssd_c55.h)* FILE NAME : ssd_c55.h ** DATE : December 19, 2011 ** AUTHOR : F...

otcagon by Associate II
  • 676 Views
  • 3 replies
  • 0 kudos

Programming guide for Stellar

Hi, Good day. This is third party for programmer.Our customer requires the programming for SR5E1-176, and we need the programming guide to develop the programming board and algorithm. Could you help to share the programming guide to me?or Please let ...

JHsu.14 by Associate II
  • 295 Views
  • 0 replies
  • 0 kudos

Resolved! StellarStudio targetting SR6G7

Hello,I want to build a simple application (like a UART message, GPIO bit-bang etc.) targeting SR6G7 and running on a custom board. To support that I want to use the latest SDK 3.3.0 and flash the code via StellarLINK.Is there any guide how to add th...

savo by Associate
  • 508 Views
  • 1 replies
  • 0 kudos

Resolved! Set Life Cycle

I am using the SPC58 MCU product with the TRACE32 debugger. When changing the Life Cycle from "customer_delivery" to "in_field" with the trace32 script, debugging is only possible by entering the keycode. What should I do if I want to change the Life...

hgh by Associate
  • 435 Views
  • 1 replies
  • 0 kudos

Resolved! How to execute demo of sensorless Field oriented control in SPC560PL5 MCU and L9907 evaluation kit. There are three demos available 1 single shunt motor control 2 standard motor control 3 thee shunt motor control

How to execute demo of sensorless Field oriented control in SPC560PL5 MCU and L9907 evaluation kit. There are three demos available1 single shunt motor control2 standard motor control3 thee shunt motor control Which one should I select for sensorless...

PT.1 by Associate II
  • 467 Views
  • 1 replies
  • 0 kudos