Very long awaited, but it is finally here!!!New AutoDevKit Studio release version 2.4.0 is available for free download www.st.com/autodevkitsw New features:- Multi-chain, multi-node and completed renovated BMS driver for L9963E named AEK-POW-BMSCHAIN...
Hi,
If you are getting this kind of error when you try to run your OpenOCD in AutoDevKit Studio 2.2.1:
Then most probably you have not updated the search path of the config files.
From main AutoDevKit menu, select Run > Debug Configurations
In th...
Dear Members.
The current BMS board design has not taken in consideration all the recommendation for a Hot Plug capable design.
To make your system hot-plug resistant make sure to follow the recommendations below:
Change the battery connector with a ...
We are releasing the first beta version of the BMS GUI for the AutoDevKit solution! Get the online update Version 2.3.1 for your AutoDevKit Studio now! Have a look at slides 4, 18, 19, 20, and 22 for details.
Let us know...
To all community members,
We are pleased to announce that we have created support for OpenOCD, a new programmer / debugger for SPC58x microcontrollers. The software is license free and you do not have any code size limitations! The new dongle AEK-MC...
Hi,
What you experience is normal because the automatic allocation will look for available pins and allocate them randomly.
If you do not want to change the wiring, then you have to manually move the pin copying EXACT name and pin configuration.
If y...
Hi,
The only example you can take is the CAN / CAN-FD driver available in source code inside AutoDevKit Studio. You could use that as a basic starting point.
The other option is to request a third-party consulting company to support you in the driver...
Hi,
Just checked with designer and the answer is that our hardware does not support CAN-TP, because we have opted for CAN-FD.
You can try to implement it in software but this means that you have to create a new CAN driver and cannot use the default o...
Hi,
I am not sure what you mean with CanTp.
If we are talking about CAN-FD, the APIs are the same, you just need to change the configuration in AutoDevKit Studio from standard CAN to CAN-FD.
Best Regards,
AutoDevKit Team