Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Where to find programming documentation

Hi ST community,I am new to SPC5 Automotive chips but not new to programming in the embedded world. I am currently programming on the SPC574k discovery board and have severe problems finding good documentation on how to actually program the thing in ...

Sir_Alee by Associate II
  • 964 Views
  • 1 replies
  • 0 kudos

SPC5 Studio Application configuration

Dear Team,           I have some doubts about How to use SPC5 Studio Application for Enabling GPIO,UART,SPI and etc. We are developing custom board using SPC582B60E1MH00Y MCU for our application. We are new for this SPC5 Controller and Studio Applica...

Priya1 by Associate
  • 882 Views
  • 0 replies
  • 0 kudos

Resolved! SPC582B60E1 Pinout Description.

Dear STMicroelectronics Support Team, I hope this message finds you well. I am currently working on a design that incorporates the SPC582B60E1MH00Y microcontroller, and I need the detailed pinout description or any supporting documentation that outli...

Priya1 by Associate
  • 1180 Views
  • 1 replies
  • 1 kudos

Basic blink led code for SPC58EE84E7

Hello,I am using SPC58EE84E7 custom board, I am able to flash the application using JTAG debugger (stellar link), Please let me where I am going wrong as the led is not blinking.Below is the configurations that I am doing to setup the project:1. 2. B...

yashg25_0-1746704799777.png
yashg25 by Associate II
  • 1053 Views
  • 1 replies
  • 0 kudos

Resolved! Stellar Studio development software is based on SR6G7.

Hello! I want to build a simple application (such as UART messages, GPIO bit flipping, etc.), with the target being SR6G7, and run it on a custom board. For this reason, I wonder what kind of work I need to do? The StellarStudio development tool has...

Leu1 by Associate
  • 1327 Views
  • 2 replies
  • 0 kudos

SPC58NH protect RAM when reset

Hello, I'm using the SPC58NH-DISP board, and my application needs to preserve some variables across a software reset — such as when the reset button is pressed or a WDT reset occurs. My application requires a warm boot feature.When I assign a value t...

Unlock JTAG programmatically by code on SPC58

Hi, I'm developing a Bootloader for SPC58, If I full secure the micro and put its LC status as In-Field on UTEST, is there a way from the internal code (I can implement a serial command for the purpose) to unlock the JTAG? Or there is no way animore?...

GMG by Associate III
  • 1439 Views
  • 2 replies
  • 0 kudos