Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Basic blink led code for SPC58EE84E7

Hello,I am using SPC58EE84E7 custom board, I am able to flash the application using JTAG debugger (stellar link), Please let me where I am going wrong as the led is not blinking.Below is the configurations that I am doing to setup the project:1. 2. B...

yashg25_0-1746704799777.png
yashg25 by Associate II
  • 1065 Views
  • 1 replies
  • 0 kudos

Resolved! Stellar Studio development software is based on SR6G7.

Hello! I want to build a simple application (such as UART messages, GPIO bit flipping, etc.), with the target being SR6G7, and run it on a custom board. For this reason, I wonder what kind of work I need to do? The StellarStudio development tool has...

Leu1 by Associate
  • 1363 Views
  • 2 replies
  • 0 kudos

SPC58NH protect RAM when reset

Hello, I'm using the SPC58NH-DISP board, and my application needs to preserve some variables across a software reset — such as when the reset button is pressed or a WDT reset occurs. My application requires a warm boot feature.When I assign a value t...

Unlock JTAG programmatically by code on SPC58

Hi, I'm developing a Bootloader for SPC58, If I full secure the micro and put its LC status as In-Field on UTEST, is there a way from the internal code (I can implement a serial command for the purpose) to unlock the JTAG? Or there is no way animore?...

GMG by Associate III
  • 1456 Views
  • 2 replies
  • 0 kudos

stellar studio

我能为此问题做些什么 似乎系统无法使用 SDKS 文件夹中的工具 Translation: "What can I do with this problem? It seems that the system cannot use the tools in the SDKS folder"  

200c99ebacd1084d0572e3e94abd71ef.png
zi_n by Associate
  • 4030 Views
  • 1 replies
  • 0 kudos

SPC5Studio SPI Generating Code for SPC574K not working

Hallo,I tried to use the DSPI_0 interface with the transfer configuration as shown in the picture, but cannot generate the necessary code with the error shown below. I could try a walkaround with byte wise frames and exchanging 4 bytes at a time but ...

grafik.png
Sir_Alee by Associate II
  • 595 Views
  • 0 replies
  • 0 kudos

Setup Output Pin for SPC582B PWM Emios

I want to generate pwm signal with spc582B with out the signal directly to pin emios0 channel 11 (uc11 pin).Already use the pwm Icu sample project. With channel 11 out, so I use group 1. When running, the periode callback is working, but still no out...

jmary by Associate III
  • 706 Views
  • 0 replies
  • 0 kudos