Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Query in FMEDA Analysis performed for SPC58xNx

We are implementing application software in performance core. So, we are bound to do FMEDA analysis,  *   Is there a FMEDA analysis performed in SPC58xNx hardware from your side?  *   All failure detections which are carried over in performance cores...

SP.4 by Associate
  • 644 Views
  • 1 replies
  • 1 kudos

Resolved! Stellar E vs Stellar P for inverter

Hello, I am interested in the Stellar E and P series for the purpose of motor control, with an inverter topology that has 12 independent switches and requires fine control of the offset between some of the waveforms.1) The E series is marketed as opt...

ay by Associate
  • 1313 Views
  • 2 replies
  • 0 kudos

SPC560P-DISP CAN TX

I've got the CAN Test app loaded and working as it should. I'm trying to get it to transmit out instead of loopback. I've already uncheck the option for loopback and simplified the code to only transmit. However, I don't see any activity on the CAN p...

BXS by Associate II
  • 1322 Views
  • 6 replies
  • 0 kudos

Getting started with SPC560P-DISP

Just got an SPC560P-DISP and I'm following AN4487 Getting started instructions. I have the board connected via USB to my computer and I've got SPC5Studio up and running with a Serial Test App. I have cleaned, generated and compiled the app. Following...

BXS by Associate II
  • 755 Views
  • 0 replies
  • 0 kudos

CAN is setting with BusOFF state

Hello Team, I am currently utilizing the SPC58EC Microcontroller in an Autosar project where I have set up the CAN MCAL driver for both Tx and Rx operations in interrupt mode. We have noticed that whenever the system bus experiences a sending bus loa...

Rajkumar by Associate
  • 1260 Views
  • 1 replies
  • 0 kudos

Resolved! STELLARLINK vs SPC5-UDESKT

Hello,​I've been looking for a debugger to debug and program an SPC58xx MCU and I've found you offer both the new Stellarlink and the SPC5-UDESKT. I understand the SPC5-UDESKT requires a licence to be used with the Universal Debug Engine (UDE) which ...

OHarc.1 by Associate II
  • 4595 Views
  • 6 replies
  • 0 kudos