cancel
Showing results for 
Search instead for 
Did you mean: 

MCU SPC560B50L5 error: “Unable to enable OnCE 10-bit TAP controller Failed to connect. Could not perform custom sequence.”

AR8000G
Associate

Hello.

I am using an MCU SPC560B50L5  in an LQFP144 package on the board, connected via JTAG. I'm trying using J-Link V11 SEGGER J-Link Registration V8.10 program.

When I try to connect, I get the error: “Unable to enable OnCE 10-bit TAP controller Failed to connect. Could not perform custom sequence.”

What to do for a ready connection?

0 REPLIES 0