cancel
Showing results for 
Search instead for 
Did you mean: 

MLC Output Delay

FKara.3
Senior

Hello,

I have recently conducted a test on the activity recognition task using the ST library with ESP32 MCU. Although it functions correctly, there are noticeable delays before action recognition occurs. I am seeking advice on how to address this issue.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
niccolò
ST Employee

Hi @FKara.3 

what do you mean by "noticeable delays"? also, if you are using the Human Activity Recognition library on microcontroller, this is not the right section, I would advise to post in the STM32 community =)

I could help you with MLC activity recognition feature as an embedded algorithm on ST sensors. there, the time depends on the algorithm itself and on the ODR of the sensor (it needs a certain amount of samples to be sure of the condition) 
also remember that every MLC activity recognition algorithm can be tuned by the user to reach the specified performances =)

If this answers your question, please, mark this as "best answer", by clicking on the "accept as solution" to help the other users of the community

Niccolò