Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[Short Survey] Please give us your feedbacks on ST model Zoo Services

Hi everyone,   In order to help our developers understand how their work is used and what to do in order to improve model zoo, we kindly ask you to look at this survey about ST Model Zoo Services.   Link of the survey: https://docs.google.com/forms/d...

Resolved! STM32N6 + YOLOv8n ONNX Model. Issues with PNG Input and Code Generation

Hi everyone,I'm working with an STM32N6 board and trying to deploy a custom YOLOv8n model in ONNX format using CubeMX and STM32 Edge AI. I’ve run into a few issues and was hoping someone could help clarify the process.Here’s what I’ve done so far:I s...

TerZer by Associate III
  • 3155 Views
  • 16 replies
  • 6 kudos

Resolved! Unanle to run tensorflow lite micro on stm32769 eval board

I am trying to run tflm with stm32f769 eval. I build the tflm as a static library and included it in my project. My app  is crashing whille calling allocatetensors() function.  Anyone having any luck with it? Also I couldn' find any official demo for...

hadi81 by Associate II
  • 859 Views
  • 3 replies
  • 0 kudos

the result of onnx model validate on target has two different output, why?

hiI have validate on the STM32N6 board by onnx model in STM32MX,but i have two different output ,like this: m_outputs_1: (10, 3)/float64, min/max=[-282.578064, 481.370483], mean/std=[-2.619613, 298.301398], output  m_outputs_2: (10, 1)/float64, min/m...

cxf by Associate III
  • 8403 Views
  • 25 replies
  • 2 kudos

STM32N6570 and storing a model in the flash

Hello! How can I store the model's input data in the flash of the STM32N6570-DK, then deploy the model, read the input data from flash, and perform inference? Are there any relevant tutorials for this? I previously followed the model deployment tutor...

llcc by Senior
  • 1768 Views
  • 5 replies
  • 1 kudos

Resolved! Problems with running an AI Model on the NUCLEO-N657X0-Q Board

Hello, I'm working with a NUCLEO-N657X0-Q Board and trying to run/debug a TensorFlow Lite model that has been quantized to int_8 to run on hardware. I've tried several approaches but every attempt leads to a dead-end of one error leading to three mor...

Coop23 by Associate
  • 2118 Views
  • 2 replies
  • 2 kudos

Resolved! Is X-Cube-AI working for N6 with NPU?

Hello,i am trying to use the NPU on the N6 by creating a project with CubeMX/X-Cube-AI. After creating the project i am greeted by a lot of errors (30). I don't change any of the code after code generation. So my question is, is X-Cube-AI with NPU ev...

LukasOst by Associate II
  • 1069 Views
  • 3 replies
  • 2 kudos