User Activity

Hi community,I'm working on deploying an object detection project using Edge Impulse on STM32H747i-DISCO with CAMS OMV. I successfully deployed the TFLite model, but I would like to add camera and board configuration to detect objects in real time. H...
Hi Community,Is there a pre-trained model for object detection, other than for people counting?
Hi Community, I’m working on deploying my custom tiny ISSIMO-V8 model for object detection onto the STM32H747I-DISCO board with the OMV CAMS camera. Can I use the FP-AI-Vision 1 project, which is based on object detection for people counting, and mod...
Hello All, I'm currently working with the STM32 H747-DISCO board, but I'm encountering some difficulties in interfacing the B-CAMS-OMV Camera Module. The LCD is functioning correctly, but the camera is not working (even though the 3 LEDs are lit). I'...