2019-02-25 02:28 AM
Dear community
We are pleased to announce the release of STM32CubeMX v5.1.0
What’s new ?
Supported STM32Cube package versions:
· STM32F0 V1.9.0
· STM32F1 V1.7.0
· STM32F2 V1.7.0
· STM32F3 V1.10.0
· STM32F4 V1.24.0
· STM32F7 V1.15.0
· STM32G0 V1.1.0
· STM32H7 V1.3.2
· STM32L0 V1.11.0
· STM32L1 V1.8.1
· STM32L4 V1.13.0
· STM32MP1 V1.0.0
· STM32WB V1.0.0
Main Fixed issues
Known limitations
Please read the Release note for the known limitations
2019-02-26 12:41 AM
Hi @Noppe.Jack
You have two ways to install STM32CubeMX:
1- from app icon
2- With Command line "java -jar STM32CubeMX-5.1.0.exe"
2019-02-26 12:48 AM
Hello @MNapi ,
You can simply ask a new question in https://community.st.com/s/topic/0TO0X000000BTr8WAG/stm32cubemx (if not already done there).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-02-26 12:50 AM
Hi @anio1491
Trying to fix a server issue
2019-02-26 03:06 AM
It is OK now you can download the FW
enjoy the 5.1.0
2019-02-26 04:29 AM
Hi @Nawres GHARBI ,
Thanks for the update. Still a lot of issues unresolved.
See this: https://community.st.com/s/question/0D50X0000APYl2qSQD/stm32cubemx-501-lpuart1-missing-nvic-menu
and this: https://community.st.com/s/question/0D50X0000APbf7ESQR/bug-in-spi-transmit- .
Regards,
Andreea
2019-02-26 06:56 AM
How to get rid of this message after generating code?
Migrated a 5.0.1 project and never used GFXSIMULATOR in my life.
I find no appropiate config setting in the file <myproject>.ioc
There is no warning when building a new project from scratch.
2019-02-26 09:47 AM
Thank you Nawres. Those files only showed up when the RC6 file was posted to the website. The original file that was released earlier in the morning did not have them.
The good news ... since RC6 all seems to be in order. I know the software is not perfect (lots of reports in the forum), but no software ever is. Overall, I find CubeMX very useful. Thank you 🙂
2019-02-26 10:09 AM
Here are my timers after playing, I get around 3.7 ms period. You must have this board on your desk and take look yourself. Those number are not correct when you try to setup in cube mx following the book. This board or the code needs some changes / improvements.
static void MX_TIM1_Init(void)
{
/* USER CODE BEGIN TIM1_Init 0 */
/* USER CODE END TIM1_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
/* USER CODE BEGIN TIM1_Init 1 */
/* USER CODE END TIM1_Init 1 */
htim1.Instance = TIM1;
htim1.Init.Prescaler = 45;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 4000;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 7;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
sConfigOC.Pulse = 1;
sConfigOC.OCPolarity = TIM_OCPOLARITY_LOW;
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
sConfigOC.Pulse = 3;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
{
Error_Handler();
}
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = 0;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
sBreakDeadTimeConfig.BreakFilter = 0;
sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
sBreakDeadTimeConfig.Break2Filter = 0;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM1_Init 2 */
/* USER CODE END TIM1_Init 2 */
HAL_TIM_MspPostInit(&htim1);
}
2019-02-26 11:59 AM
I'd would like to see some Documentation on this GFXSimulator and what it is intended to be used for. I've searched and have found nothing on it.
Thanks
2019-04-04 09:53 AM
@Nawres GHARBI - Where is CubeMX plug-in 5.1? I'm trying to use this within Atollic.
I downloaded the software on this page: https://www.st.com/en/development-tools/stm32cubemx.html
Unfortunately that seems to be only the stand-alone executable, no plugin ZIP.
Thanks!