2019-02-25 02:28 AM
Dear community
We are pleased to announce the release of STM32CubeMX v5.1.0
What’s new ?
Supported STM32Cube package versions:
· STM32F0 V1.9.0
· STM32F1 V1.7.0
· STM32F2 V1.7.0
· STM32F3 V1.10.0
· STM32F4 V1.24.0
· STM32F7 V1.15.0
· STM32G0 V1.1.0
· STM32H7 V1.3.2
· STM32L0 V1.11.0
· STM32L1 V1.8.1
· STM32L4 V1.13.0
· STM32MP1 V1.0.0
· STM32WB V1.0.0
Main Fixed issues
Known limitations
Please read the Release note for the known limitations
2019-02-25 06:44 AM
@Nawres GHARBI How do we access the bug tracker where the details of the CubeMX fixed and outstanding issues are explained?
2019-02-25 07:05 AM
Nawres, I suspect there might be something wrong with the package for MacOS
2019-02-25 08:38 AM
@Nawres GHARBI It would be great if you would post these announcements AFTER the stuff is actually available on the web site (unless you intend to annoy your customers 😉
2019-02-25 08:59 AM
Hello,
I was able to update my CubeMX (finally) to the release today (v5.1.0), but I am not able to update the L0 firmware package to the lastest version. I can see that there is a new packet available, but the download fails, and therefore, I cannot generate anymore code.
Any idea on what's wrong?
Please see screenshots attached.
Regards,
Andreea
2019-02-25 10:39 AM
When I setup PWM or OC clocks for example I did setup the main clock in Clube MX 50 Mhz
I used 50 divider to get 1 MHz instead I was getting something like 490 KHz. They were pretty close but never close. Like the main oscillator was not accurate.
When I did 25 divider I got like 990 KHz. I do have oscilloscope connected to the pins so I can see what is coming out.
I cannot see doing any mistake all looks simple and straightforward in Cube MX
But still if I do 50 MHz in Cube Mx shouldn't I get
RCC_OscInitStruct.PLL.PLLN = 50;
instead of
RCC_OscInitStruct.PLL.PLLN = 25;
2019-02-25 11:30 AM
Can we trust RC6 or should I wait for a final release?
2019-02-26 12:11 AM
could you please attach the used ioc
2019-02-26 12:13 AM
Hi @Dave Nadler
The bug tracker isn't accessible for the moment but it is planned to be in the future
2019-02-26 12:15 AM
Hi @Dave Nadler
The package was available on the web site when the post has been published, it may sometimes have a little late to appear to you depending on the web synchronization
2019-02-26 12:17 AM
Hi @Joerg Wagner
The RC6 is the final release for 5.1.0