STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Configure USART3 at STM32MP157D-DK1

Hello Friends, I am trying to configure USART3 as UART full duplex on the STM32MP157 evaluation board. The pin configuration for USART seems to be working correctly, but I’m having trouble with the USART3 Control Register1 & BRR . Can anyone help me ...

B_D_R by Associate III
  • 2507 Views
  • 9 replies
  • 0 kudos

Resolved! Can STM32MP135 run FreeRTOS?

Hello,I am using the STM32MP135DAF7 chip for bare metal development, and now I have encountered a problem. Specifically, I have transplanted the FreeRTOS system on this chip, and in the boot_develop mode, I can run FreeRTOS normally, that is, ddr_ini...

LYUhaha by Associate II
  • 1498 Views
  • 2 replies
  • 0 kudos

STM32mp1 yocto project

Hi, I'm new to yocto project,while building core  minimal image , my Linux PC got shutdown bcoz of low battery , after restarting it , trying to use bitbake command , but it shows command not found , Do i Need to again  build the environment by sourc...

Anto_Z by Associate II
  • 3604 Views
  • 4 replies
  • 2 kudos