STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157 unable to boot from SD

As part of our project, we are using an STM32MP157DAC custom board that has the same design with the STM32MP157D-DK1 development board except for a few changes (schematics of the design is attached)The board generally works when trying to upload and ...

shobole by Associate
  • 1057 Views
  • 2 replies
  • 0 kudos

Resolved! uint8_t Values Are Not Changing

 I want to download and use firmware (FW) to DDR3. Since DDR is initially disabled, the firmware to activate DDR and the main FW project are separate, and the download procedure is as follows:First, run the DDR activation FW to enable DDR.Download th...

Stnoobs by Associate II
  • 2343 Views
  • 12 replies
  • 0 kudos

Resolved! PROBLEM: first boot STM32MP257F-EV1

I'm trying to perform the first boot on the STM32MP257F-EV1 following this guide: STM32MP25 Evaluation boards - Starter Package.  I've connected the LCD screen to the board according to the instructions.The board is powered by USB-C on CN21, and the ...

Zim by Associate II
  • 1822 Views
  • 6 replies
  • 0 kudos