STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

openamp: OpenAMP_TTY_echo

Hello!If I run the openAMP example I can see the two new devices appear in the linux /dev folder: ttyRPMSG0 and ttyRPMSG1, so that's fine!I would like to give these entries another name, like instead ofttyRPMSG0 --> KEYSttyRPMSG1 --> FRAMQuestion 1: ...

EOF by Associate III
  • 504 Views
  • 0 replies
  • 0 kudos

Teseo-Liv4F

Hello, We are evaluating the X-STM32MP-GNSS1 eval board on STM32MP-157F-DK2.The X-STM32MP-GNSS1 has Teseo-LIV3F GPS receiver on it, which does not support NAVIC.Since we want to test receiving signals from NAVIC specifically, can we replace the Teseo...

Quad SPI Transmit issue

 I'm working with the STM32MP131FAE in a bare-metal environment, and I'm experiencing issues with QuadSPI.I want to use Quad SPI to send 96 bytes of data continuously without any clock interruptions.However, currently, the data is being sent in chunk...

Stnoobs_0-1731320053002.png
Stnoobs by Associate II
  • 462 Views
  • 0 replies
  • 0 kudos