Hello,I have a STM32MP157C-DK2 board and did the hello world cross compile project with GTK and that work perfectly.Now I am trying to do cross compiling with Qt Creator. I used the same compiler as the GTK project but Qt Creator give me an error: Th...
I have just bought an STM32MP157C-DK2 and would like to get started. I found a tool within the wiki which allowed me to select a bunch of the "getting started" sections and create a PDF. However. all the pages of the PDF just said I didn't not have p...
Hi,I am only a bit familiar with embedded linux. I will develop a demo project with STM32MP157C-DK2 with C language:on M4 side, a sensor(BME280) and a vantilator (5v) are connected. Sensor is to read periodically and three numerical values( temp, hum...
stm32-ipcc 4x001000.mailbox: Try increasing MBOX_QUEUE_LEN remoteproc remoteproc0: stm32_rproc_kick: failed [vql, err: -105) Hey all,I'm working with the OpenSTLinux EGLIFS QT image, and having issues running the OpenAMP TTY Echo program.When I ...
sed: can't read /home/letter/new-development/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/ncurses-native/6.1+20180630-r0/sysroot-destdir/home/letter/new-development/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/ncurses-...
Hello, I trying to make the example in: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4/Modify,_rebuild_and_reload_a_firmwarebut after SSH password window (here i put root in pass...
Hi, I used the below link for building OpenSTLinux Distribution.https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package As mentioned in the step 7 "Flashing the built image", there should be a /deploy/image folder for images. But i didn't fin...