cancel
Showing results for 
Search instead for 
Did you mean: 

Dear All, in STM32MP15x application notes I found capacitor parallel with the battery(VBAT pin) . I would like to know what is the practical reason to place capacitor next to a chemical battery? Maybe that capacitor can be omitted? Regards, PL

Lacc
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hi,

it depend on your battery size and technology, if chosen battery has relatively low internal resistance during life time (roughly < 50ohms like a CR2032 coin cell), capacitor could be skipped.

Although current on VBAT is very small in many cases, there is some small peak of current (due to RTC activity or active TAMP pins toggling) which might need to be filtered by the capacitor, especially when the battery is near their end of life. The capacitor might increase (a bit) the time where the low-bat is detected by your system.

Capacitor type should be carefully checked to avoid additional leakage which might ruin the battery lifetime (especially at high temperatures).

Even if not intended for that purpose, capacitor is useful as additional ESD protection when battery is swapped without care by the user.

Very large capacitor could also help to maintain VBAT in case of battery swapping (but this is not the main goal, and large capacitor might have more leakage).

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here