2020-12-02 8:51 PM
Hello ST Support team,
I have MP23DB01HP digital MEMS MIC sensor which has PDM output. I was gone through "AN5027" application note.
I want to connect this digital MIC with DK2 to find dB data from it.
suggest me steps to connect and run mic on DK2 board.
Thanks in advance,
Nikunj
2020-12-03 12:46 AM
Hi @NPanc.1 ,
On DK2, It is possible to connect digital MEMS MIC to the 40pins connector (SPI5 and SAI2 are available).
Nevertheless, the recommanded way to connect digital MEMS MIC is using DFSDM IP, but this is only available on EV1 board with its dedicated connector (connector 2 in the picture).
I woudl suggest the following steps :
BR,
Christophe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.