STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Multiple Endpoints on A7 and M4

Hello,iam trying to implement more or less the same example as with the virtualUARTs with multiple Endpoints just with the rpmsg_char driver and plain endpoints without virtualUART on M4 side. Iam struggling to get multiple Endpoints to work. One is ...

YRink.1 by Associate II
  • 2880 Views
  • 4 replies
  • 0 kudos

Resolved! I've come across the chip ID caveat mentioned in the op-tee documentation for secure storage. Are unique chip IDs implemented in STs branch of the op-tee OS? Also is trustzone code itself stored securely at rest or only the data in secure storage? Thanks

Full text from op-tee: Important caveats Currently no OP-TEE platform is able to support retrieval of the Hardware Unique Key or Chip ID required for secure operation.   For all platforms, a constant key is used, resulting in no protection against de...

Hello, I am trying to execute a simple ADC program(12bit) in stm32mp157c using trimpot with 10K as input in cube ide. Where output changes only at the voltage level of 3.2v

While changing the value at the trimpot output values is constant(4095) and has no change as soon as when it reaches 3.2V it goes to zero. I am seeing output using uart. ​Please assist me how to rectify it.​

ASuha.1 by Associate
  • 625 Views
  • 1 replies
  • 0 kudos

Resolved! I have been following the instructions on the wiki to set up STM32CubeProgrammer on dk2. It appears I am missing port parameters. What is the correct command line?

I enter STM32_Programmer_CLI -c port=/dev/bus/usb/010/003 (lsusb reports this is correct) -w flashlayout_st-image-weston/trusted/Flashlayout_sdcard_stm32mp157c-dk2-trusted.tsvudev drivers installed, Ubuntu 20.04Warning: Wrong connect parameter:

SLetter by Associate III
  • 1594 Views
  • 9 replies
  • 0 kudos