STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LAN8720 Device Tree changes

HI all,We are using LAN8720 as the ethernet PHY for connectivity.The IC has 25MHz crystal connected for the refclk and we want to run in RMII mode. We have requirement of not using the INT_N for the ethernet IC.Upon exploring the ST Docs I was not ab...

NPal.2 by Senior
  • 796 Views
  • 1 replies
  • 0 kudos

Resolved! Pinout/Functionality between STM32MP1 devices and development boards, are they mostly similar?

Hello,I would like to embark on a project for a custom board with the STM32MP157DAB1 and I am referencing the STM32MP15-DISCO schematic from ST which uses the STM32MP157CAC3.My Question: How do I translate between the functionality of the pins?From o...

0693W00000Hqit7QAB.png
daded.1 by Associate II
  • 1474 Views
  • 3 replies
  • 0 kudos